Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Mazatrol Smooth C-problem with Thread cycle (turn machine)

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi,

 

we have problem with thread cycle on turn machine.

We don´t know how to create PP for thread cycle.

This is the error:

Zajeta slika.PNG

See attachment file (G code).

Can somebody help me?

6 REPLIES 6

Re: Mazatrol Smooth C-problem with Thread cycle (turn machine)

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I don't see the attachment.

Note older (E and I series Integrexes) used a 2 line format for threading (G276 on the machines I've dealt with), but it looks like they've changed things on your machine.

Mazak QTN I have a manual for also uses 2 lines (but with G76)

Do you have the docs for the G76 cycle? 
Can you (legally) post them? 

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Mazatrol Smooth C-problem with Thread cycle (turn machine)

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

this is the g code.

 

I don´t have nothing else, that is the problem.

Re: Mazatrol Smooth C-problem with Thread cycle (turn machine)

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Without having the EIA programming docs for your machine, it is hard to say.

Is this a new machine?  Or did you buy it used?

Have you (last couple years) bought a new Mazak machine from the local Mazak Distributor?

Maybe see if (if you give them the model / serial number) they could hunt down an appropriate EIA manual?

 

Until then, I'd post lathe threading as individual G3x lines - it could be that G76 is a drill/bore cycle, not threading...

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Mazatrol Smooth C-problem with Thread cycle (turn machine)

Valued Contributor
Valued Contributor

What does the "D" in your code stand for?

 

I think thread line should look as follows...

G76 X...Z...R...P...Q...F...

 

You might wanna use Vargus CNC Prog Gen for illustration.

 

Kal.

 

 

 

NX 9.0.3.4 MP12 | PB 9.0.3.2 | NX11.0.2.7 MP13 | PB 11.0.2 | VERICUT 7.3.4

Re: Mazatrol Smooth C-problem with Thread cycle (turn machine)

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
It s working.
Thanks a lot.

Re: Mazatrol Smooth C-problem with Thread cycle (turn machine)

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
Hi,

What it means R, P and Q?

Learn online





Solution Information