Cancel
Showing results for 
Search instead for 
Did you mean: 

Merging CAM resources

Honored Contributor
Honored Contributor

We use NX 9, and TC 10, at two different sites, with one Teamcenter database, and utilizing the NXcustom setup developed by Rob Cohon.  Most users have been setup like this for about 2 years now, except for the machine shop at the other facility.  Now, as the NX admin/non CAM guy,  I have been tasked to assymilate them in with everyone else.  For the most part this has been pretty straight forward, but now I am finding various files on their native setup, that I think I need to merge into our network location, and I'm not 100% sure how to do this.

 

Example, the tool database files in resource\library\tool\english.  Is there a way to merge these, and not lose info from either site?  or do I have to create group folders for each site?  Ideally, I *think* we want one location for everything.

 

Same for the machine_database.dat file.

 

Any insight would be appreciated.

 

 

 

 

-Dave
NX 11 testing NX1847+ | Teamcenter 11 | Windows 10
8 REPLIES 8

Re: Merging CAM resources

It sounds like your libraries are in native, so based on that...

 

If the sites will be sharing the same libraries, then you need to merge them manually. Be careful not to duplicate librefs. 

 

If they will keep separate libraries, you cound use separate CAM configurations, or just use separate resource areas.

 

In native, I would have a resource folder for each of them, and then set UGII_CAM_RESOURCE_DIR differently at each site. You could have the same resource area, and only have separate libraries, but that is a little harder to set up. For me the duplication is worth less headaches.

 

Mark Rief
Retired Siemens

Re: Merging CAM resources

Honored Contributor
Honored Contributor

We do have seperate groups for Indy and NC, so that might be the easiest way to do this.

 

Thanks Mark!

-Dave
NX 11 testing NX1847+ | Teamcenter 11 | Windows 10

Re: Merging CAM resources

There are also performance considerations if there is slow access to the resource folder, since this is where the libraries and template parts are.

Mark Rief
Retired Siemens

Re: Merging CAM resources

Honored Contributor
Honored Contributor

We are also looking at the MRL (Manufacturing Resource LIbrary, since it appears the Kennametal catalog is available for it.

 

Since I am just starting this journey, is there anyting I can do now with these libraries, that would help the move to MRL?  or is it a complete start over?

-Dave
NX 11 testing NX1847+ | Teamcenter 11 | Windows 10

Re: Merging CAM resources

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

MRL is a complete start over, since it is best to avoid anything you have introduced in the past that might be a problem in the future.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: Merging CAM resources

Honored Contributor
Honored Contributor

FYI, GTAC informed me about the "Convet Tool Library" function, which is supposed to convert your custom files:

 

tool_database.dat

holder_database.dat

segmented_tool_database.dat

trackpoint_database.dat

 

It's worked for 2, maybe 3 of the 4.  One is unchanged, so I can't tell if anything changed.  GTAC is trying to figure out why the 4th didn't merge.

-Dave
NX 11 testing NX1847+ | Teamcenter 11 | Windows 10

Re: Merging CAM resources


@DaveK wrote:

FYI, GTAC informed me about the "Convet Tool Library" function, which is supposed to convert your custom files:

 

tool_database.dat

holder_database.dat

segmented_tool_database.dat

trackpoint_database.dat

 

It's worked for 2, maybe 3 of the 4.  One is unchanged, so I can't tell if anything changed.  GTAC is trying to figure out why the 4th didn't merge.


This should work if you did not change the classification or add fields to the data records.

If you added tools to the existing classes, then those should all be converted to the format of the newer release. If you modified our out of the box tools, those changes are ignored.

Mark Rief
Retired Siemens

Re: Merging CAM resources

Honored Contributor
Honored Contributor

I have passed that along, since I didn't create any of the tools, I have no idea what the machine shops may have done, if they know...a lot of this was setup by Siemens initially.

 

It's in a testing phase right now, waiting to hear back from the machine shops.

-Dave
NX 11 testing NX1847+ | Teamcenter 11 | Windows 10

Learn online





Solution Information