03-06-2018 06:27 AM
Good Morning,
I am looking for a base post processor to make a save-as of.
I am creating a metric probing post for an Okuma (Renishaw Ins Plus). All my previous probing posts have been in Inch format but now I require a metric one I cannot see any anywhere.
There are none in the MACH OOTB folder and there are none on the GTAC download page.
Does anyone have any ideas?
03-06-2018 09:18 AM
If you are using Post Builder, if you have a post with one units, and you need to support the other units, you can:
"Output Settings" tab -> "Other Options" tab -> specify an "Optioinal Alternate Units Subpost"
I've never used it, but there should be docs on it, and it should get you what you need...
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled
03-07-2018 10:04 AM
Ken,
Thanks for your response. I have set up this alternate sub-post and it seems to function well at this early stage. I will see how it develops.