Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Milling of a Slot on 5axis

Valued Contributor
Valued Contributor

Hi 

I want to mill a slot (Red Coloured) on 5 axis with 8mm endmill . Please any one guide me how i do create its tool path in NX 12.

I am attaching part file with my post.....aaa.JPG

 

 

 

6 REPLIES 6

Re: Milling of a Slot on 5axis

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

here you are

I fix your attempt contour profile :

only one wall, one floor, not auxiliary geometry, align to edges tool axis

And add one operation:

variable contour curve/point method, offset curve left parameter, normal to part, cut area specified

 

*projection vector, collision checking , engage is up to you

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: Milling of a Slot on 5axis

Valued Contributor
Valued Contributor

@Juraj 

thank you for your replying on my post.... tool path is making round portion at the entry of slot...is it possible to make sharp edges on the floor of the slot at the entry as it is in the exit? thank you.Capture.JPG

Re: Milling of a Slot on 5axis

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
You need nonrotary tool, like turning cutter and - broach motions. I did a same.

Re: Milling of a Slot on 5axis

Siemens Phenom Siemens Phenom
Siemens Phenom

 

I did this in 1851, but here are the steps in case you are on a lower version.

 

1) Create a new Variable Contour operation, select face of slot for workpiece in operation, do not use the solid body.

ScreenHunter 109.png

 

2) Change Drive Method to Curve/Point, pick inside bottom edge as drive curve. In Drive Settings set Offset Left and Tool Contact Shift to 4mm

ScreenHunter 111.png

 

3) Generate

ScreenHunter 112.png

Re: Milling of a Slot on 5axis

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Just wondering (and being too lazy to open the file)

As you get to the outer rim, won't your spindle contact (collide with) the rim on the other side?

Or is this a head rotary axis machine (and the whole head fits within the "bowl" of the part?)

Or are you using some sort of angular head so the spindle clears the part?

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Milling of a Slot on 5axis

Siemens Phenom Siemens Phenom
Siemens Phenom

I change the projection vector and tool axis, it now clears...

Unable to play video. Please try again later.
(view in My Videos)

Learn online





Solution Information