Cancel
Showing results for 
Search instead for 
Did you mean: 

Milling "closed" groove in side wall

Experimenter
Experimenter

Hi,

I have been reading and seeking alot of help on this forum, but this is my first post.

I have run into trouble when trying to cut a simple groove in the side of a block with a slot cutter, I am not able to find an operation that works. I have tried the "Groove Milling" operation but that only seems to work when the groove runs thoughout the completer side of the wall. If I try to select the modeled groove I only get an error message telling me that a groove feature can not be derived from the selected geometry.

 

If there's anyone out there can give me any pointers in the right direction it would be highly appreciated.

 

Best regards,

Gustav

 

Capture.JPG

2 REPLIES 2

Re: Milling "closed" groove in side wall

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

You could use floor-wall milling, since that supports undercut milling with t-cutters.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX12.0.2, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX (1876) | AWC 3.4 Preparing: -

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: Milling "closed" groove in side wall

Siemens Phenom Siemens Phenom
Siemens Phenom

the attached NX12 part file uses both planar_profile and floor_wall wiuth Allow Undercut turned on

Learn online





Solution Information