Cancel
Showing results for 
Search instead for 
Did you mean: 

Mix toolpath

Builder
Builder
Hello friends
Anybody knows that how to mix two toolpath...otherwise any new strategy

if total cutting level 150mm

Than from top side to depth 100mm(cut level (depth 100mm)) is Z-Level profile and from depth 100 to 150 is Cavity mill...so how to merge this in allover one toolpath

6 REPLIES 6

Re: Mix toolpath

Phenom
Phenom

merge your 2 operations in program > generate the cls into a working directory of your choice (edit the clsf with Notepad delete the first "END OF PATH" and the 2nd "TOOL PATH/")> menu > tool > import clsf > replay toolpath  Smiley Very HappySmiley Very Happy

Sorry it's not possible in a associative way

Production: NX11.0.2.7,VERICUT 8.1.2
Development: Tcl/Tk, Gnuplot
www.adgroupe.com

Re: Mix toolpath

Siemens Phenom Siemens Phenom
Siemens Phenom

We currently are in development with a Merge toolpath project. 

 

Please feel free to contact @Eddy_Finaro if you are interested in testing this functionality.

 

Cheers,

Alexander

Lead Product Manager - Mold & Die
Highlighted

Re: Mix toolpath

Siemens Phenom Siemens Phenom
Siemens Phenom

Alexander is right. Starting at NX1847 (major release next to NX12) you will be able to select two or more operations and merge them into one special program group somehow like Optimized_NC in Hole Making. it will support several merging rules i.e.

  • Concantenation - operations are merged in sequence, but if the end of a certain operation is close to the begining of next - the connection will be on the cut area in a smooth manner.  
  • By Contour - in the simple version 1st contour from 1st operation is performed, then 1st contour from 2nd operation, 3rd operation etc. till the last operation and then 2nd contour from 1st operation etc.
  • By contour will also allow merging a semi-finish operation having 10 leves and a finish operation having 50 levels such that after the first semifinish pass - 5 finishing passes will perform before going to the next depth. 
  • the infrastructure allows to add more merge rules as needed.

(this solution is of course associative and can be used as part of your templates..)

It is available in the EAP versions if someone is interested in trying it out and report back feedback.  

 

@Vora - does this seem to address your initial request?

 

Yours,

Eddy Finaro
NX CAM Product Manager
Siemens PLM

Re: Mix toolpath

Experimenter
Experimenter

Eddy,

I am also interested in this functionality.  Is it possible for you to provide detailed instructions?  I am currently working with FCA milling groups evaluating NX1847 functionality and this is something they indicated they need.

Thank You,

fred Brender

Re: Mix toolpath

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Fred,

 

you do not need a special teplate. it is part of the OOTB instalation. create a new Program Group, select and type - mill_multi-axis or mill_mult-Blade and select the (new) Merge path option:

Merge_Path.jpg

also - documentation should be part of the instalation. if you have questions - please let me know.

you may also want to watch the tech-tip Merge Tool Paths

 

Yours,

 

Eddy Finaro
NX CAM Product Manager
Siemens PLM

Re: Mix toolpath

Experimenter
Experimenter

Got it...thanks.  This is exactly what we're looking for!

Learn online





Solution Information