Cancel
Showing results for 
Search instead for 
Did you mean: 

Modify I-J-k and G68

Pioneer
Pioneer

Hello,

 

I have a problem with modifying the from G68.2 to G68.1 and from I angle-Jangle-Kangle to I vector-Jvector-Kvector(I mean with vector I0 J1 K0).

I try to explain it with below pic.

Can anyone help me please?

 

g68.png

g68-1.png

3 REPLIES 3

Re: Modify I-J-k and G68

Gears Phenom Gears Phenom
Gears Phenom

hi,

as far as I know

in G68.2 IJK are euler angles

in G68.1 (G68?) by ijk select axis rotation and R is angle of rotation.

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: Modify I-J-k and G68

Pioneer
Pioneer

Thank you,

 

Actually i know what they are, my question is ;

 

the post which i have is posting G68.2 and I,J,K with angle,

 

I want to change this codes from G68.2 to G68.1 and from I,J,K angle to I,J,K vector in the post with post builder. 

Re: Modify I-J-k and G68

Gears Phenom Gears Phenom
Gears Phenom

I assume you have to do it twice, for example:

g68.1 i0j0k1 R-90

g68.1 i0j1k0 R90

 

if yor question is how to do it, you have to find where this block (g68.2) is called, create new 2 blocks and call them.

if you want more detailed clue how to operate postbuilder, tempate blocks, etc - I recommend to watch videos about postbuilder https://community.plm.automation.siemens.com/t5/Tech-Tips-Knowledge-Base-NX-Manufacturing/tkb-p/open...

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Learn online





Solution Information