Cancel
Showing results for 
Search instead for 
Did you mean: 

Modify post by Post Builder to get one file for each operation

Creator
Creator

Hello,

 

Using Post Builder I would like to modify my post so that when I select a group of operations the post will generate

a separate file for each operation. Each filename should be equal to respective operation name. 

Attached zip file includes .def, .tcl, .pui and the actual iso file that is produced when I select a group of 5 operations.

 

Anyone can help ?

 

1 REPLY

Re: Modify post by Post Builder to get one file for each operation

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello,

 

the OOTB example sim03 is working that way, it creates for each operation an extra subprogram plus one main program which is calling the multiple subprograms.

If you open that file you can check it:

sim03_mill_4ax_cam_sinumerik_tombstone.prt

 

On top of the post builder post we provide in the meanwhile an Post Configurator post too.

 

Thomas Schulz
Siemens PLM
Manufacturing Engineering Software

Learn online





Solution Information