Cancel
Showing results for 
Search instead for 
Did you mean: 

Modify the ISV Behaviour to machine "upside-down"

Siemens Creator Siemens Creator
Siemens Creator

Hi everyone,

 

Im trying to force an ISV (GROB 550 - 5 axis table table nutating) change the way it machines to behave more like it does in production. The one we have had a modification in the CYCLE800 so that everytime it is called it has a preference to rotate the table -180 so the part is upside-down most of the time.

 

So far i understand iv'e got to make changes to the CSE Driver files, I tryed modifying the ToolChange.SPF file adding a A-180, it works for the first operation, but it doesn't stick afterwards (i do understand why), so I need a different solution, what im thinking is changin the CYCLE800, I just dont know how.

 

Does anyone have an idea?

5 REPLIES 5

Re: Modify the ISV Behaviour to machine "upside-down"

Legend
Legend

I have a Grob G350....

Why are you moving the table at Tool change?
The whole advantage of the Grob is you can leave the table still and grab a new tool.

 


Dennis Rathi
Creations Unlimited

Re: Modify the ISV Behaviour to machine "upside-down"

Siemens Phenom Siemens Phenom
Siemens Phenom

The cycle800 itself picks the solution.

 

From my understanding is your described problem a topic how the picker selects between two possible solutions. The internal CSE function checks if two solutions exists (based on the limits). If two exists, like in your case both are delivered  or better provided to the cycle and the NC code of the cycle800 itself takes care which one is picked. With the ISV CSE simulation (today) you use the OOTB shipped cycle as part of the SinumerikSL_Cycles.cyc file. That is based on Sinumerik Version 4.4.

 

You can check the limits of the axis to influence the picked solution. Also check the values of the TC_CARR variables so that they fully match the one from your machine tool. In the OOTB Example they are defined inside the file TC_DEFF.DEF

 

Hope it helps

 

Thomas Schulz
Siemens PLM
Manufacturing Engineering Software

Re: Modify the ISV Behaviour to machine "upside-down"

Siemens Creator Siemens Creator
Siemens Creator

Maybe I wasn't that clear, moving the table at Tool change was an idea to force the GROB to work upside-down, I am modifying the behaviour of the ISV, to match to what ours does. And as I said, the change probably needs to be made at the CYCLE800 where the table reorients to have the next working face normal to the splindle, and what I need is for the new CSY to be inverted, hope this make it clearer

Re: Modify the ISV Behaviour to machine "upside-down"

Legend
Legend

My post writer made a UDE for me to work upside down. Its to select the alternate solution. Maybe you could do this? Working upside all the time  isn't a good plan unless you always make small parts because the travel upside down in y is not equal to travel normal. Maybe G550 is better about this?


Dennis Rathi
Creations Unlimited

Re: Modify the ISV Behaviour to machine "upside-down"

Siemens Creator Siemens Creator
Siemens Creator
Yes! I think that will work perfectly for what we need, can you share that UDE? Or a source of reference to write it?

Thanks!

Learn online





Solution Information