Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Multi Passes in Contour Area

Legend
Legend

Hello,

 

In the past I remember being able to set cut depths when Multiple Passes was selected. Has the dialog changed?Where are the depths of cut specified? The help docs describe an Increment option, which I remember using, but is not there anymore.

 

 

 

multi pass2.PNGmulti pass3.PNGmulti pass1.PNG

Glenn Balon
Production: NX 12.0.2 MP7 Primarily CAM
4 REPLIES 4

Re: Multi Passes in Contour Area

Gears Phenom Gears Phenom
Gears Phenom

Hi,

I have this options available.

Guiding curves method doesnt currently have it.

NX 12.0.2.9 MP3

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: Multi Passes in Contour Area

Legend
Legend

@Juraj

 

Thanks for responding. 

 

I am on same version. Do you see different dialog in your operation? A way to set the depth of cut/increment?

 

I even right clicked operation>object> customize, and updated from template thinking it would solve it. Still looks the same. 

 

NX 12.0.2.9 MP3, 16Oct18. See Maintenance Pack letter for detailed list of fixes.
NX 12.0.2.9

Glenn Balon
Production: NX 12.0.2 MP7 Primarily CAM

Betreff: Multi Passes in Contour Area

Valued Contributor
Valued Contributor

Hi

I think in the area milling setting your "Stepover Applied" is "On Part"

Set this value to "On Plane" an the checkbox should appear.

 

2018-11-05_17h59_56.png

 

 


Production: {NX 10.0.3.5 MP18}
Testing: {NX 12.0.2.9 MP03}

Betreff: Multi Passes in Contour Area

Legend
Legend

Yes, that was it. It needs to be "On Plane." 

 

It would be better if they left it there, but greyed out. Then when you hover mouse over it, it would have a message saying "must use Stepover "On Plane for this function."

 

 

How else would I have known that. I don't use it often, so I never correlated the connection between the two. 

 

multi pass4.PNGMulti-Depth Cut workingmulti pass5.PNGOn Plane

Glenn Balon
Production: NX 12.0.2 MP7 Primarily CAM

Learn online





Solution Information