Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Multi Processing / Threading in NX CAM

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Hello Everyone,

 

Is anyone aware about the current status of the Multi Processing / Threading in NX CAM.

 

  1. What is the current status of Parallel generate ?  Are there some improvements/enhancements ?
  2. What is the current status of Multithread in a single operation? (I last heard that iw was started with Multi Threading in NX 9 and wanted further to integrate i more)
  3. Is multithread active for all operation types in NX CAM or ?

Thanks in advance for your answers.

Laher

1 REPLY

Re: Multi Processing / Threading in NX CAM

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
  1. Parallel generate was already using multiple processors by spanning multiple processes in NX 7.5, you just had to set a customer default. With NX 8.5 this was improved for automatic separation, the customer default is still needed to specify the maximum number of processors/cores to use.
  2. The whats new guide and the Siemens PLM Americas connection should include a slide about the time savings when generating cavity milling, z-level profile and some other operation types.
  3. ISV has a big performance improvement in NX 10
  4. 3D verify has a big performance improvement in NX 10

If you check the what's new guide of each NX release, you should get plenty of information about performance improvements Smiley Wink

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Learn online





Solution Information