Cancel
Showing results for 
Search instead for 
Did you mean: 

Multiple instances of variables?

Experimenter
Experimenter

I'm assuming (for the moment) this issue isn't unique to just me, but so far I haven't been able to find any info concerning it.

 

When examining a posted program using the Post Review Tool, I've noticed that events frequently have multiple instances of identical variables, but with different values. For example, I'm looking at a MOM_initial_move event, and there are two instances of each variable in the mom_pos array. In this case specifically, mom_pos(2) has two different values.

 

Does anyone know exactly what is happening during run-time in this situation? Can I safely assume that only one of them is ever valid, and the others can be ignored completely?

It will be greatly appreciated if someone can clear this up for me.

 

2 REPLIES 2

Re: Multiple instances of variables?

Phenom
Phenom

The review tool shows a sequential dump of variables changing. The lower one should represent the value the event handler code will get for the event.

NX12.02
Windows 10 Pro
ITC Inc.

Re: Multiple instances of variables?

Experimenter
Experimenter
I suspected that might be the case. Thanks!

Learn online





Solution Information