Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Multiple tracking points from MRL

Creator
Creator

Hi

 

I need multiple tracking points for chamfer tool. Using user defined tool and planar profile.

I have defined 3 tracking points in MRL but in NX i see only two, why is that?

first one is missing.

 

NX value.JPGTC value.JPG

NX 11.02 MP9
TC 10.1.7
MRL 3.16
3 REPLIES 3

Re: Multiple tracking points from MRL

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

The tool tip is only used to calculate the rest of the tracking points.

To get three tracking points, you need to set up four tracking points in MRL.

The first two might be identical, if the first tracking point is also the tool tip.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: Multiple tracking points from MRL

Creator
Creator

Thank you. we'll set more points to teamcenter.

NX 11.02 MP9
TC 10.1.7
MRL 3.16

Re: Multiple tracking points from MRL

Siemens Genius Siemens Genius
Siemens Genius

Hi!

 

Stefan is right.

You can add more fields to the tracking point attributes.

Then you can have more than two TPs in NX CAM.

Up to 15 TP fields are supported in the MRL TCL file.

 

It is possible to increase the number of TP attribute values interactively.

But it is probably easier to do it on comment line.

 

Here are the two commands you can use to do that:

1.    Increase array size of the class attribute:
smlutility -add_class_attr -u= -p= -g= -cid=CLASSID -attr_id=-450xx -array=10
2.    Increase array size of the default view attribute:
smlutility -add_view_attr -u= -p= -g= -cid=CLASSID -attr_id=-450xx -view_type=Default -array=10 -recurse

 

Hope this helps...

 

   Markus

Learn online





Solution Information