Cancel
Showing results for 
Search instead for 
Did you mean: 

NC file names posted from Sync Manager

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hello

I would like to ask if there is any way to change way of naming NC files post-processed in Sync Manager.

 

By default it outputs:

myname_channel_1.ptp
myname_channel_2.ptp

 

I would like to have:

myname_K1
myname_K2
(without any file extension)

 

 

Marek Pawlus, NCmatic

Production: NX 12.0.1
Development: C#, Tcl/Tk, CSE
3 REPLIES

Re: NC file names posted from Sync Manager

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

With enough tcl magic should be able to be done.

Another option is to just (after sync manager is done) copy them to the file names you want (and leave the originals alone). 

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: NC file names posted from Sync Manager

Phenom
Phenom

Neither pops up in the info window in sync manager mode - so moving or renaming or setting the output file path in tcl are all possible. Sync manager run through on the post is separate for each channel - so it posts once completely for each side.

NX10.03
Windows 7 Pro

Re: NC file names posted from Sync Manager

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Thank you

If there is no option designed to do that, I think the easiest (and safest) way is to let postprocessor make a copy of files and rename it automatically.

Marek Pawlus, NCmatic

Production: NX 12.0.1
Development: C#, Tcl/Tk, CSE

Learn online





Solution Information