Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

(NEED HELP) machining V groove

Creator
Creator

I am trying to machine V groove  with chamfering tool (90 deg 1/4 dia )... and cant get it to work???

 

Inked60999_ass_LI.jpg

8 REPLIES 8

Re: (NEED HELP) machining V groove

Phenom
Phenom

@NX75_Ray  you didn't say what you have tried, but give planar profile a go. It is a low-level operation and will do exactly what you tell it to.

 

/Harri

 

Re: (NEED HELP) machining V groove

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Planar mill

- boundary = single edge (watch climb/conventional and side of tool when picking which one)

- floor = bottom of V

- engage = linear, in line with cut

- retract = pull out vertically, no "extension"

 

 

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: (NEED HELP) machining V groove

PLM World Member Legend PLM World Member Legend
PLM World Member Legend
Generic motion will be a good option
Patrick Delisse
KMWE - Aero Engine
NX 12.0, TC 11.2, CAMPOST V22, Vericut 8.2, TDM 4.8
C#, VB, .NET

Re: (NEED HELP) machining V groove

Creator
Creator

Hello, you want the tool path like this, right?1.png2.png

Re: (NEED HELP) machining V groove

Creator
Creator

That worked ... Thank you

I wish there was a way to turn of tool compestation ..so it would go in a middle of that groove 

2019-02-21 (2).png

Re: (NEED HELP) machining V groove

Creator
Creator

top..Yes, thats how i want toolpath to look like ....how?

Re: (NEED HELP) machining V groove

Creator
Creator

Hello,  you need to use plane contour milling for processing
Part boundaries use "guide lines" and specify planes, tool alignment
Finally, the bottom surface is also defined by the cutting method and the infeed parameters and the position of the lower knife.

Re: (NEED HELP) machining V groove

Creator
Creator
Can you share your PRT with me?



After operating the tool path, it will be provided to you.

Learn online





Solution Information