Showing results for 
Search instead for 
Do you mean 
Reply
Solved! Go to solution

NURBS motion output

Hello,

 

I am trying to make a finishing operation using NURBS motion output type in a complex part and when I try to simulate the machine movements, the following message appears:

 

problem_nurbs.png

 

Does anyone know what this 'SD' variable is and how I can fix it?

 

Thank you!

 

5 REPLIES

Re: NURBS motion output

The motion output in the operation is set to Nurbs - correct? This is a Fanuc format.

What machine/control are you using for simulation? 

Mark Rief
Retired Siemens

Re: NURBS motion output

Yes, it is set to Nurbs, with Join Segments as well (Angle tolerance: 1.0; Fitting tolerance: 0.025).

 

The machine uses a Siemens control. Should I be using a different motion output type to run in this machine? My goal is to use a polynomial interpolation.

Solution
Solution
Accepted by topic author iprestes
‎06-26-2017 08:19 AM

Re: NURBS motion output

Change the motion output to Sinumerik Spline.

If you don't see the output you want, check the post. If it is Post Builder, you may need to edit PB_CMD_init_nurbs and set it to SIEMENS_POLY.

Mark Rief
Retired Siemens

Re: NURBS motion output

Sinumerik Spline lead me to the same error message.

Apparently it was the Post Builder, since it was set to "BSPLINE". I changed PB_CMD_init_nurbs to "SIEMENS_POLY", as shown in the picture attached.

 

And also added the command PB_CMD_nurb_poly in the NURBS Move, which wasn't there (picture attached).

 

Then I tried to post process the trajectories with nurbs movement and I got this message:

Received an error 1770007

File name: o:ugnx110\ip33\camsmom\no\ind\mom_tcl_definitions.c, line number: 1255

Error message: Cannot open file

 

Should I change something else in the Post Builder?

 

 

 

 

Re: NURBS motion output

I just restarted the program and now it worked! Thank you very much!

Learn online





Solution Information