Cancel
Showing results for 
Search instead for 
Did you mean: 

NX 10.0.3 Fix contour

Solution Partner Builder Solution Partner Builder
Solution Partner Builder

Dear all 

 

I am using NX 10.0.3 . I create fix contour operation . use step over on part at 5 mm . When I generate  tool path out put  has space error (see in attach file).  This is error of program ?

 

 

thank you 

 

 

2 REPLIES 2
Highlighted

Re: NX 10.0.3 Fix contour

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

This is no error, since you selected "step on part", which takes the draft angle of faces into account.

 

If you want equally spaced steps despite of the draft angle of the faces, you need to use "step on plane".

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX12.0.2, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX (1876) | AWC 3.4 Preparing: -

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: NX 10.0.3 Fix contour

There is proabably some point alont the passes where they are going across a steep area, so they are moved closer together to maintain the stepover along the steep wall. But since zig and zig-zag patterns have parallel passes, the passes bunch together closer than this on the near flat areas.

 

 

Mark Rief
Retired Siemens

Learn online





Solution Information