Cancel
Showing results for 
Search instead for 
Did you mean: 

NX 11 CAM performance issues

Experimenter
Experimenter

First off I am new to the NX software and any insight will be great.

I am currently having an issue when selected features say to do Hole MIlling.

I get a long lag time between selections. After selecting one hole it just sits and thinks for 10-15 seconds before I am able to select the next feature. We upgraded the RAM in this computer with no benifit.

What part of the computer would affect this?(cpu,gpu ect.)

 

Thanks!

 

ps. I will say our GPU is a lower end product at the moment

7 REPLIES

Re: NX 11 CAM performance issues

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

How many faces does the body consist of?

Selecting a hole will create a machining feature in the background, which results in this delay.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: NX 11 CAM performance issues

Experimenter
Experimenter
The part its self is a very simple plate consisting of 20-30 drill holes and counter bores .
Would running the find features before hand improve this delay I am having?

Re: NX 11 CAM performance issues

Siemens Phenom Siemens Phenom
Siemens Phenom

There will be a short delay (couple of seconds, no more) when you pick the first feature.

After that, the recognition should be almost instantaneous unless you have a very complex part which doesn't seem to be the issue in your case.

 

Can you share the part so that we can validate if it's just your environment?

 

Tom van 't Erve

NX CAM Development

Re: NX 11 CAM performance issues

Experimenter
Experimenter

We work off of the server here and I just tried it working off of the SSD on this computer and was much more responsive.

Could that just be the issue?

I tried to attach a .prt file but it wouldn't let me.

 

Thanks,

Joe Pena

Re: NX 11 CAM performance issues

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Pack the part file into a compressed archive, like 7-zip or ZIP, before you upload it.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: NX 11 CAM performance issues

Experimenter
Experimenter

Here we go.

Re: NX 11 CAM performance issues

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Hello JLEP,

 

here are 2 small Videos in real Time.

HP Z Book 17 G2 32GB RAMIntel Core i7 4710 @2.5GHz

 

Regards

 

Frank

Leiter Consulting Fertigung ComputerKomplett Ascad GmbH

Learn online





Solution Information