Cancel
Showing results for 
Search instead for 
Did you mean: 

NX 11 INSTANCES

Experimenter
Experimenter

Question is, is there any way to move an INSTANCE into a different dropdown program folder without moving the original but still be linked with the original? What I’m wanting to do is:

-take the original tool path

-create an instance (mirror through plane)

-rotate the instance by whatever degree I need

-put it into a different location than the original

-post out the originals as one program

-post out the instances as another program

 

I’m wanting it to stay linked to the original that way if I make a change it will also change the instance toolpath.

4 REPLIES

Re: NX 11 INSTANCES

Legend
Legend

Straight and to the point... no

 

Smiley Sad

 

NX11.0.1

Re: NX 11 INSTANCES

Experimenter
Experimenter

Thanks for the quick reply. Guess i'll quit wasting my time with it then.

Re: NX 11 INSTANCES

Experimenter
Experimenter

Do you know any other way to copy a toolpath and keep it associated with the original?

Re: NX 11 INSTANCES

Legend
Legend

Paste with reference will do what you are asking but I've not been completely stoked with its results. It needs more development. That being said I have a lot of horizontal parts using it running....

 

NX11.0.1

Learn online





Solution Information