Cancel
Showing results for 
Search instead for 
Did you mean: 

NX 12 Boundary Creation

Pioneer
Pioneer

Is there any way to lock tool position to ON or TANTO before selecting the boundary? You were able to in older versions. If not, this is an extremely cumbersome task. I have hundreds of boundaries that have to be selected in the default TANTO position, then I have to go back and select each boundary and group select each member and make them ON.

2 REPLIES 2

Re: NX 12 Boundary Creation

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

I would also appriciate an answer from Siemens.  It is extra work to go back and edit a boundary member to change it from Tanto to ON.  This is a function that is very often needed in the real world.

 

John Joyce, Manufacturing Engineer,
Senior Aerospace

NX 11.0.2.7 Vericut 8.0.3 - Statements and opinions are mine alone and do not reflect
the opinion of my employer or any other member of the human race

Re: NX 12 Boundary Creation

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi all,

 

I'd like to give you an update on this issue. 

 

This is currently being adressed and it will be available in the version after NX12.0.2.

 

Thank you for your feedback and giving us notice :-)

 

Cheers,

Alexander 

Lead Product Manager - Mold & Die

Learn online





Solution Information