Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: NX 1847

Legend
Legend

oh yeah Smiley Very Happy


Dennis Rathi
Creations Unlimited

Re: NX 1847

Gears Phenom Gears Phenom
Gears Phenom

Hello @Eddy_Finaro , just a quick question about -  Region coolant for operation

 

I use for cooling almost own UDE instead of default NX coolant ude.

First question -

Is it possible to call it for regions own coolant?

Or do I have to read default nx coolant variables and then set my procedure according to it?

 

Second question - If so,  can I extend region coolant with other coolant types?

 

Thank you

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: NX 1847

Siemens Legend Siemens Legend
Siemens Legend

Hi Juraj,

 

I attended some discussions where this topic was raised, but the one who drives it and would know how to answer this question is @AlexanderF .

 

Yours,

Eddy Finaro
NX CAM Product Manager
Siemens PLM

Re: NX 1847

Phenom
Phenom

Anyone got a link to what's new in 1847? The help file is in the 3GB range and don't feel like downloading it just for checking the goodies..

 

/Harri

Re: NX 1847

Gears Phenom Gears Phenom
Gears Phenom

@hjoy

https://docs.plm.automation.siemens.com/tdoc/nx/1847/nx_help#uid:index_whatsnew

 

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: NX 1847

Phenom
Phenom

Thanks @Juraj!

Re: NX 1847

Phenom
Phenom

Oh wow, what a lot of nice new stuff! Hope it's stable and without new serious bugs Smiley Wink

Re: NX 1847

Gears Phenom Gears Phenom
Gears Phenom

@Eddy_Finaro do you mean @AlexanderFreund ?

Because person you mentioned wasnt logged since 2017.

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: NX 1847

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @Juraj,

 

no, you currently can't add a customized command, but you can change the M command for the various option we currently have. We added a new section for this in the Postconfigurator.

 

Cheers,

Alexander

Lead Product Manager - Mold & Die

Re: NX 1847

Gears Phenom Gears Phenom
Gears Phenom

Hi, thanks for answer @AlexanderFreund

but what if some machine has more coolant types than only "ON,Flood,Mist,Thru,Tap and new - AIR, AIR_THRU?

Just asking Smiley Happy .Because Ive met machines that has more coolant types + pressure settings - many combinations = many M.. codes. And I handled it by custom UDE coolant.

 

In postbuilder I can also react on variables - I can create extra coolant array member for M code, this is not a problem - if we are talking about adding new coolant types to default ones.

 

So some enhancement show up? - possibility to add more options in UI to that region coolant or possibility to call  own user event?

 

 

-ps.: I stopped using default coolant ude long time ago because of some coded logic with ON option - dont want that or any restricions.

 

cheers

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Learn online





Solution Information