Cancel
Showing results for 
Search instead for 
Did you mean: 

NX 8.5 turning

Genius
Genius

I have some problems with setting grooving operations.

1.I'm trying to reduce radial safe clearance value for tool retracting from the cut, (non cutting moves/clearance/workpiece clearance) but minimum tool clearance is 1mm even when I add radial safe clearance value 0mm, OD and ID cutting.

2.Even when I add trim planes for some reason tool is gouging into the part.

 

2.png

 

 

1.png

 

3.In cone grooving when I check additional profiling and pick diameters first, then faces, or something else, nothing happens cutting parameters are not taken into the account?

 

Learn online





Solution Information