Cancel
Showing results for 
Search instead for 
Did you mean: 

NX 9.0.3 MP2

Solution Partner Builder Solution Partner Builder
Solution Partner Builder

HI

 

 I have some problem in NX 9.0.3 MP2  . When I simulate machine ( machine code simulation program is alarm (see in attach file )  when I use NX 9.0.2 not alarm .  and i can not use function simulate machine code file ( When I choose G code file and click OK  not has anything . in NX 9.0.2 It show display simulation control panel .

 

 

thank a lot

 

7 REPLIES 7

Re: NX 9.0.3 MP2

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

Hi 22,

 

I assume you´ve updated your kinematic model with the new axis and channel properties and you´ve forgotten to assign the spindle to the channel.

 

ThomasF

 

spindle_assignment.png

Machine Tool Enablement
Manufacturing Engineering Software

Re: NX 9.0.3 MP2

Solution Partner Builder Solution Partner Builder
Solution Partner Builder
Thank.

Ok. I check this box at you recommend . But it not solve my problem. Do you have a new method ti solve it ?

Re: NX 9.0.3 MP2

Legend
Legend

Make channel name as numbers e.g. 1 (String like “Main” will cause the problem)

Re: NX 9.0.3 MP2

Solution Partner Builder Solution Partner Builder
Solution Partner Builder
Thank

Where is the channel name ? I can not find .


thank .

Re: NX 9.0.3 MP2

Solution Partner Builder Solution Partner Builder
Solution Partner Builder

OK

Now I can use machine code simulation  .  But when I use simulate machine code file . now it has two channels ( in attach file )  What is the input in channel  to run simulate machine code ?

 

 

thank

Re: NX 9.0.3 MP2

Legend
Legend

How many channel you have on the machine?

First channel should be defined as "1" ; second "2" ..

If you have 2 channels the external code simulation ask you for 2 files -- one for the first channel and the other for the second channel.

Re: NX 9.0.3 MP2

Siemens Phenom Siemens Phenom
Siemens Phenom

The problem with the two channels is an already know and reported problem. Development is working to solve it.

 

 

Thomas Schulz
Siemens PLM
Manufacturing Engineering Software

Learn online





Solution Information