Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

NX 9 Customizing Resource Bar

Experimenter
Experimenter

I recently moved to a laptop with a docking station and I want to find a way to get the operation navigator, part navigator, and assembly navigators to switch positions when going from single to multiple monitors and vice versa.

 

This happens in all modes but manufacturing is where I spend the majority of my time. I have already tried setting up two seperate roles, but the position of the navigators don't go from the second monitor to the primary monitor when I change inbetween them.

 

Is there any way to do this?

2 REPLIES 2

Re: NX 9 Customizing Resource Bar

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I think window positions are stored in the registry (assuming you are Windows).

You may have to save 2 REG files of "HKEY_CURRENT_USER\Software\Unigraphics Solutions\NX\9.0"  (possibly you can limit them to just some of the sub-keys).

 

Or try to "reset window position" before loadiing your role?

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: NX 9 Customizing Resource Bar

I'm not sure what you can do in NX9, but in NX10 there are new options for the resource bar preference:

  • Overlap on Second Monitor
  • Dock on Second Monitor

 

Mark Rief
Retired Siemens

Learn online





Solution Information