Cancel
Showing results for 
Search instead for 
Did you mean: 

NX CAM DEMO

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hello all,

 

  I want to do a CAM demo on 3 axis. can anyone provide the supporting documents or how to achieve this?

 

 

 

Any ppt would be helpful or parts for demo

5 REPLIES

Re: NX CAM DEMO

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Have you checked the CAM tutorials shipping with NX ?

Have you checked the samples at "%UGII_BASE_DIR%\MACH\samples" ?

From my experience as a customer, it is best to request a sample part from the customer the demo is done for and use that for the demo.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: NX CAM DEMO

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Thank you @Stefan_Pendl.

 

I will look into it. 

 

 

 

 

Re: NX CAM DEMO

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
So the operations which comes under mill contour are used for 3 axis right?

Yes, that's right, this covers 3-axis level-based machining and fixed axis surface contouring.

You can check out the CAM tutorials from within NX manufacturing through the button shown below.CAM_Tutorials.PNGCAM Tutorials

This will open the initial page in the NX internal browser window of the resource bar. I would think the die and high speed machining are the ones that are most appropriate in your situation.

If you use the sample part file "cam_sample_mill_contour" and its setup part, you should be able to create a simple demo of machining a part from blank to finished Smiley Wink

Make sure to use rough step sizes to reduce calculation time depending on your demo machine.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: NX CAM DEMO

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

In addition I would also show them floor wall, which is now a good way for roughing.

If you still got time, you should also give adaptive milling a go, but you should mention that this is the initial phase and that there is more to come through the NX 12 release cycle.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: NX CAM DEMO

Siemens Genius Siemens Genius
Siemens Genius

Hello

 

From MBG we provide an extensive NX CAM Demo environment, which you can find on salescenter here:

MBG NX CAM Demo Environment v5.4 for NX11.0.2

 

It contains around 20 CAM demos of various kind.

 

Best regards

Lars Okkels

Siemens Industry Software

Best regards

Lars Okkels
Siemens, MBG

Learn online





Solution Information