11-29-2016 04:22 AM
Hi,
we have a 3 axis CNC machine: spinner-MVC-850 / Sinumeric 840 D SL-710-6A2C.
I want to know if it is possible to use mill_3axis_Sinumerik_840D_mm.pui as a post processor for this machine without any customization or I must do a customization to generate the G code to this machine.
I want to know if there is an other post processor for this machine in the postprocessor library and it needs customization or not.
Could you please help.
Thanks .
Regards.
11-29-2016 04:27 AM
There is no way to avoid customization, since every machine tool vendor adds his own stuff.
All the PPs shipping with NX are good for a start, but they all need to be adapted to fit the machine.
You can buy two machines of the same kind and configuration about half a year apart, but they are different in their innards.
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0
Employees of the customers, together we are strong
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide
11-29-2016 04:40 AM
11-29-2016 09:30 AM
11-29-2016 10:43 AM
Yes - coolant codes (particularly for high pressure) often change machine to machine.
Another issue is if some machines have an option, and some don't
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled
12-07-2016 04:27 AM
Thanks