Cancel
Showing results for 
Search instead for 
Did you mean: 

NX CAM SUBROUTINE

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hi all,
I would not consult anyone from nx to generate NC code for a subroutine Fanuc if a solution is to postbuilderu?


Thank you all for any help

2 REPLIES 2

Re: NX CAM SUBROUTINE

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Are your asking how to post somethings as a Fanuc style subroutine?
(i.e. end the posted output with M99 instead of M2 or M30)?

 

Or are you asking how to call a subroutine?

 

Or are you asking how to post a long program as a "main" program file + "subroutine" files?

 

And are you asking for Post Builder solution or Post Configurator?

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: NX CAM SUBROUTINE

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

I'm concerned about solutions to postbuilderu. When I have one operation and is used for several zero points (G54-G59) so that listed at the end of a subroutine of the operation and at the beginning it was invoked at every zero point (G54-G55), depending on the datum.

Learn online





Solution Information