Cancel
Showing results for 
Search instead for 
Did you mean: 

[NX CAM-Turning] extend cut region

Solution Partner Innovator Solution Partner Innovator
Solution Partner Innovator

Hi

 

I doing turning operation. cut region is shown bellow.

region.jpg

 

When creating the tool path, it is generated as below.

 

tool_path1.jpg

 

Each separated area is an X value of the same diameter.

So I want to create a linked tool path.

 

tool_path2.jpg

 

Is there an option?

 

2 REPLIES 2

Re: [NX CAM-Turning] extend cut region

Siemens Phenom Siemens Phenom
Siemens Phenom

If you uncheck Update IPW in the gooveing operation NX thinks the materail is still there. The ROUGH_TURN_OD operation machines it. I tried using Ignor Member in Custom Part Boundary Data, but got the same result as you showed.1.gif2.gif3.gif4.gif

Re: [NX CAM-Turning] extend cut region

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Another option is to add "blank" stock (probably radial in this case) (cutting parameters -> stock tab).

Make it more than the groove depth.

Note it will add blank stock to the ENTIRE model, so you may have to use "cut region" containment to NOT cut other areas.

I'm not sure if you can use "custom boundary data" to add stock to just the groove elements of the boundary.

 

Yet another option is to use teach mode to do an "axial" move from the start point to the end point. (If you try "profile" it will still break it into different sections)

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Learn online





Solution Information