Cancel
Showing results for 
Search instead for 
Did you mean: 

NX CAM

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi Any Body,

 

whether NX Cam can support for making plasma cutting program?

 

Thank you

Dadang

4 REPLIES

Re: NX CAM

Gears Phenom Gears Phenom
Gears Phenom

My quick answer is yes.  Could you post an example of what your looking for?

John Joyce, Manufacturing Engineer,
Senior Aerospace

NX 11.0.2.7 Vericut 8.0.3 - Statements and opinions are mine alone and do not reflect
the opinion of my employer or any other member of the human race

Re: NX CAM

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
Hi Joyce,
Thanks for your prompt response.

My customer want to make integration all process using one system from Design to manufacturing process.
For First step they ask whether NX Cam can support for their plasma cutting machine.

I checked it in cam configuration and template part file, there is lasert part template.
I tried to use it but the error massage “ No record found” appear.

My question are : What should I do so that laser template can be used?
Is it the similar between plasma cutting with laser cutting program?

Re: NX CAM

Gears Phenom Gears Phenom
Gears Phenom

To the best of my knowledge NX does not have a "Plasma" or " Laser" cutting operation. 

 

I have see people use Planar Mill and Wire - EDM operations to create a tool path for this and other 2 axis cutting equipment.  The truly important thing will be a post processor to format the NC code. 

 

 

My question are : What should I do so that laser template can be used?  - Contact GTAC
Is it the similar between plasma cutting with laser cutting program?  - Without an example of what the NC  code looks like it would not be possible for me to answer.

 

If you have an example of he NC code your looking to create then post it here.

 

John Joyce, Manufacturing Engineer,
Senior Aerospace

NX 11.0.2.7 Vericut 8.0.3 - Statements and opinions are mine alone and do not reflect
the opinion of my employer or any other member of the human race

Re: NX CAM

Siemens Legend Siemens Legend
Siemens Legend

The Laser Template you see was an early attempt by Siemens in developing 5 axis laser functionality. It never even made it to the preview stage.

For plasma cutting ( I am assumimng 2 1/2 axis ), I would start by using planar profile operations and letting the post with some custom UDEs to controll all specific commands.

Learn online





Solution Information