Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

NX CMM: Easy way to copy and pattern bolt hole circles

Pioneer
Pioneer

As the title suggests, if i have a bolt hole circle whats the best way to copy the first bolt hole and pattern it around a diameter at a given angle so that all the holes are inspected the same way and i dont have to select each hole individually?

 

 

39 REPLIES 39

Re: NX CMM: Easy way to copy and pattern bolt hole circles

Pioneer
Pioneer

Anyone?

Re: NX CMM: Easy way to copy and pattern bolt hole circles

Where exactly in the system you are making the selection?

Mark Rief
Retired Siemens

Re: NX CMM: Easy way to copy and pattern bolt hole circles

Pioneer
Pioneer

what do you mean?

 

i have a bolt circle made up of 40 holes.

 

how do i write a program so that all the holes are inspected without me having to take the time to select each and every hole?

Re: NX CMM: Easy way to copy and pattern bolt hole circles

Pioneer
Pioneer

bumps

 

in PCDMIS i have the ability to copy a circle and then pattern it around at a desired angle and quantity.

 

does NX CMM have the same ability somewhere? PATTERN doesnt seem to work for me (or at least i havent figured it out.)

Re: NX CMM: Easy way to copy and pattern bolt hole circles

Pioneer
Pioneer

bumps

Re: NX CMM: Easy way to copy and pattern bolt hole circles

Pioneer
Pioneer

Re: NX CMM: Easy way to copy and pattern bolt hole circles

Phenom
Phenom

I dont have a licence for or use CMM.

 

In normal CAM it is possible to instance an operation

 

Transform

Re: NX CMM: Easy way to copy and pattern bolt hole circles

Pioneer
Pioneer

cool.

 

but i need NX CMM solutions. thanks for trying though.

Re: NX CMM: Easy way to copy and pattern bolt hole circles

Siemens Pioneer Siemens Pioneer
Siemens Pioneer

You can right click on the inspection path and choose transform to instance that path. Or, if you have a PMI callout with all the holes selected, you can use link to PMI and it will path all the holes. One other option is a probram called Hole Blaster that will select all the holes on the face.

 

 

Learn online





Solution Information