Cancel
Showing results for 
Search instead for 
Did you mean: 

NX CMM: Is there anyone on this forum actually programming using NX CMM?

Pioneer
Pioneer

or am I the only one?

6 REPLIES

Re: NX CMM: Is there anyone on this forum actually programming using NX CMM?

Gears Legend Gears Legend
Gears Legend
At our company we have tried it, but stopped once it was clear that the dmis output is the only format thats supported. Our Zeiss machines cant handle dmis. Zeiss had a converter for dmis to calypso, but it was so limited, that most of the probes and sensors had to be recreated after the conversion.
This was at the NX8 period
Patrick Delisse
KMWE - DutchAero
NX 12.0, TC 11.2, CAMPOST V22, Vericut 8.1, TDM 4.8
C#, VB, .NET

Re: NX CMM: Is there anyone on this forum actually programming using NX CMM?

Valued Contributor
Valued Contributor

Are you programming just cmm's or doing some machine probing as well?

 

I have looked at machine probing a little in nx11 beta and it looks promising for us but I need to work on a post and capturing data before I make a decision on buying it.

NX 12.0.1

Re: NX CMM: Is there anyone on this forum actually programming using NX CMM?

Pioneer
Pioneer

programming just CMM.

Re: NX CMM: Is there anyone on this forum actually programming using NX CMM?

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Dear Paehv,

 

at the time of NX8 the supported way to execute inspection plans on Zeiss CMMs was to export DMIS to Calypso. This was is not the supported way any more, we have another way, called CMM Inspection Execution. With this solution, you are able to execute DMIS plans as they were created in NX CMM on Zeiss machine without any problem. You need the Zeiss CMM-OS instead of Calypso configured to be able to go this way.

 

Regards,

Máté

Re: NX CMM: Is there anyone on this forum actually programming using NX CMM?

Experimenter
Experimenter
Can anyone answer this question? Can NX inspection be used for machine tool probing and not just CMM probing? In other words can NX inspection output be configured to be posted on a regular machine tool like an 840D sl control?

Re: NX CMM: Is there anyone on this forum actually programming using NX CMM?

Valued Contributor
Valued Contributor

Yes, I have proved out a probing workflow in our company to create Fanuc type probing programs, execute them and capture results data so at this point I am just waiting for final purchase approval.  We have not done this for Siemens controls but I noticed there are Siemens probing cycles in the NX postprocessor folder. 

NX 12.0.1

Learn online





Solution Information