Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

NX Cam 12.0.2 doesn't work after running

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Hi !

 

I have a problem with running NX Cam Express 12.0.2 after installation. I installed the software as usual. After running, NX turns off after a few seconds... I tried reinstalling NX, but problem persists. I reinstall the PC Operating System after the recommendation, but problem persists.

I've found that the problem is to load the NX start page. If I turn on NX multiple times, the software works normally.

I found these errors in the system log:

Error.PNG

 

In the attachment file is a video to see this my problem.

Do you have any experience with it? Do you know how I should proceed?

 

Thanks for your advise and answers.

Best regards, Jakub.

 

2 REPLIES 2

Re: NX Cam 12.0.2 doesn't work after running

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

As a guess, your user.mtx, dialogmemory, and/or registry settings got hosed.

Both the following steps assume NX12.

1) Close NX and all related applications (post builder, external translators, etc.)

2) I would rename the user folder where NX gets the files from (typically "C:\Users\YOUR_USERNAME\AppData\Local\Siemens\NX120"

3) Save, then delete, the registry key

HKEY_CURRENT_USER\SOFTWARE\Unigraphics Solutions\NX\12.0

4) try starting NX again

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: NX Cam 12.0.2 doesn't work after running

Solution Partner Creator Solution Partner Creator
Solution Partner Creator
Hi Ken_A !

Thanks, problem solved. I cleaned the registry and reinstalled Windows 10 update.

Learn online





Solution Information