Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

NX Help

Valued Contributor
Valued Contributor

Having trouble accessing NX help since Company upgraded our Computers to Win 7. If I go to help file locations looks like everything is there, also went from IE to Google Chrome as it crashes a lot less, is there a setting that needs changed ?

Mike

NX 11.0.2.7
Win 10
3 REPLIES

Re: NX Help

Valued Contributor
Valued Contributor

You can try UGII_UGDOC_BASE_DIR. You can also check where it points to now in the logfile. 

 

 

W10 NX12.0.2.9
testing v1847

Re: NX Help

Genius
Genius

Hi,

 

We had a similar problem and it was down to what Java version you are using and the security permissions, I think there is something about this on the GTAC site somewhere.

 

Give them a shout, hope they sort something out for you.

 

Cheers

 

Dave  

Regards

Dave
NX10.0.3MP13
NX11.0.1
Production
TC10
Vericut 7.3,7.4.1,8.0.2

Re: NX Help

There are several SFBs related to java updates and their effect on searching in the documentation. I would start with SFB-Teamcenter-8157, which lists all the others.

 

The good news is you won't have to deal with this in NX10.

Mark Rief
Retired Siemens

Learn online





Solution Information