Cancel
Showing results for 
Search instead for 
Did you mean: 

NX ISV MetaCode "G20 HP=1" "TD=010015"

Experimenter
Experimenter

Dear All

 

I am working on an Okuma MillTurn Simulation, and I have these machine Code in the NC file, which could not be recognized by the controler.

 

(1) G20 HP=1.  Always with the error "Parse error after reading 'G20 HP='.   I have tried to create "G20" as the metacode, and define the "HP" as the <MCParam>.......and it wont work any way....

 

Do you guys have any experience to handle this code?    I just want it to pass me a variable with the value "1" or other values.   It seems that "="  is the cause for the parse error.

 

Or is there anyway I can just skip this block for the simulation.   I tried to define "G20" as "Do nothing"...but the parse error is always there.

 

(2) TD=010015.   Same parse error as above, I think that is the "=" caused the error.   I want to get the tool number and offset number from the block.

 

Please let me know if you have any suggestion.

 

 

1 REPLY 1

Re: NX ISV MetaCode "G20 HP=1" "TD=010015"

Siemens Phenom Siemens Phenom
Siemens Phenom

Are you using the Okuma.CCF?  As I can simulate these two NC blocks with the OOTB sim05 Okuma example.

 

Thomas Schulz
Siemens PLM
Manufacturing Engineering Software

Learn online





Solution Information