Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

NX Machine Configurator : 1 Value -> 2 Axis

Creator
Creator

Hello Community, 


in my CAM Model I have an U and X Axis. These two should move with the same values that are stored with the X-Axis in the G-Code. I added to the Machine Configurator the Addresses X and tried to customize it.

Here is a picture of the xml file for X:

 xml_file_U_X.PNG

It seems like it is the wrong syntax. When i start a symulation, i get this errorerror.PNG

do you now how to make sure that the U and X Axis are moved with the values that

are stored with the X-Axis ? 
Thank you. 

2 REPLIES 2

Re: NX Machine Configurator : 1 Value -> 2 Axis

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

 

with the SetJointValue command you can set only one value to one axis per call. In your case you have to set the joint value to U and X axis with 2 command calls.

 

Thomas

Re: NX Machine Configurator : 1 Value -> 2 Axis

Creator
Creator

Thanks, it worked.

Learn online





Solution Information