09-29-2015 09:26 PM
Dear,
i want to patch all hole and pocket to manufacturing them, to help me improve time, but i don't know this tool and how to make the same picture, please help me!
09-30-2015 01:10 AM
Sync Modeling, DeletecFace. + Bounded Plane.
09-30-2015 01:41 AM
09-30-2015 02:13 AM
09-30-2015 06:45 AM
Which NX version are you using ?
There are commands which are from Mold Wizard now in Synch. Modeling. You can use these to close the open areas which are not 'holes'. For holes and counterbores, use delete hole command in one go.
BR,
10-02-2015 03:21 PM
The part in the picture on the right contains a split surface used for die design. If that is your intent, you need something from outside NX CAM like tooling or plain modeling. Synchronous would not help achieving this.
If your intention is to get rid of the holes in order to perform some roughing, then you have two simple options:
A: Use synchronous Delete Face (with optional holes setting). This modifies an existing solid body.
B: Use the Patch Openings command. This adds additional sheet bodies to the existing solid body of the part.
In both cases you should WAVE link the solid body of the part to your cam part.
You seem to be kind of at the beginning of your tour through NX so better stick to option A.
11-06-2017 05:19 PM - edited 11-06-2017 05:38 PM
Hello @Nguyennhotu
Normally the tool tries to cut inside the holes, pockets... which causes unsteady toolpath and unwanted machining time.
I think; in that case you should use ''Patch Openings'' command; when you patch these holes or pockets... the pool will not try to engage the holes or pockets... and you'll get a smooth toolpath like in the picture below.
A tip: When you create the patch surfaces don't forget to add these surfaces to the workpiece or cutting face of operation.
Here is the link which i found very helpful from AllyPlm:
https://allyplm.com/2015/05/tip-of-week-may-15/
Regards.Smooth Toolpath with Patch Surfaces