Cancel
Showing results for 
Search instead for 
Did you mean: 

NX Probe module

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hi everyone,

I know UG probe as below image, Do you know in UG there is another probe module

 

probe.png

6 REPLIES 6

Re: NX Probe module

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I'm not sure if this is your question, but...

There is "on machine probing", which (I think) is meant for when you are probing with an standard NC machine (mill/etc.), with Renishaw (or whatever) probing macros added.

Then there is NX CMM programming module(s), which (I think) is for programming actual CMMs (Zeiss/Mitutoyo/etc.)

 

If not, could you be more specific?

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: NX Probe module

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

on machine probing belong NX or the third party

Re: NX Probe module

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I believe on-machine pobing belongs to NX.

It utilizes Generic motion with specific "motion types" (probe point, probe web, etc.)

Then as part of posting, the "probe point" (or whatever) event gets converted to the appopriate call (Renishaw or other)

 

 

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: NX Probe module

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Note the Renishaw "Perfect part" software has an NX interface (that uses Generic Motion) that you may have to buy from them(Renshaw) to get the correct GM event types...

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Highlighted

Re: NX Probe module

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

What are you looking for? 

 

The probing in NX can be customized in the post.  I think it is designed to support the Rennishaw inspection Plus routines. 

John Joyce, Manufacturing Engineer,
Senior Aerospace

NX 11.0.2.7 Vericut 8.0.3 - Statements and opinions are mine alone and do not reflect
the opinion of my employer or any other member of the human race

Re: NX Probe module

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

At TTL we have created Probing Plus, which is an extension of the NX on machine probing module. There is an overview here: 

 

 http://www.ttl-solutions.com/probingplus

Learn online





Solution Information