Cancel
Showing results for 
Search instead for 
Did you mean: 

NX Simulation

Pioneer
Pioneer
 
TOOL is invading PIECE
UNDER THAT IS HEAD 25
TABLET 10 CORTE
AFTER PASSING THE CUTTING HEIGHT
THE HEAD it invades IF I
INCREASED CUTTING HEIGHT
SHE DOES THE SAME THING JA CHANGED THE TOLERANCE OF IPW
And no avail CHANGED THE MEASURE TO STEM
24.9 TAMBEM no avail
3 REPLIES

Re: NX Simulation

I don't understand your question. 

Can you describe it differently? Or maybe contact GTAC so that they can look at it with you?

Mark Rief
Retired Siemens

Re: NX Simulation

Pioneer
Pioneer
invasao.jpg 
I'm sending the image
the invasion could not solve
already moved up to the tolerance of ipw but not forward
I changed the stem diameter
and also not solved

Re: NX Simulation

Legend
Legend

the problem is not the simulation.

Since there is a collision and the collision is detected, simulation is doing its job.

You sized down the shank to 24.9 but the collision is far more bigger than 0.05mm so is still detected.

The problem is in the toolpath, there are lower contour profiles that remove more material than upper ones, causing the collision between the ipw and the tool shank.

You have to modify the toolpath to prevent the collision.

To better explain the point I've prepared this video:

 

https://youtu.be/eyNmVFIeZ08

 

have a nice day

ciao

Learn online





Solution Information