Cancel
Showing results for 
Search instead for 
Did you mean: 

NX and Hyper Threading

Phenom
Phenom

I Purchased a new Dell workstation recently.

 

In the past the recommendation was to disable Hyper Threading as it would impact performance.

 

Is this still true?

 

Thanks

 

Alex

 

NX4.0.4.2 MP10 (yes still, for some automated processes)

NX9.0.3.4 MP12 

Windows 7 pro 64

Dell Precision T7910

Dual Intel(R) Xeon(R) CPU E5-2637 v4 @ 3.50GHz

64GB RAM, Quadro M4000

5 REPLIES

Re: NX and Hyper Threading

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Have not seen that recommendation any more, but since you are using an ancient NX release too, you will have to check on your own, if turning HT on will have negative impact on NX 4.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: NX and Hyper Threading

Legend
Legend

Hi Alex,

 

Like a Stefan, I have not seen that recommendation any more for CAD and CAM.

 

But for CAE, this still true, as you can see in the NX 9.0 On-line Help in link below.

https://support.industrysoftware.automation.siemens.com/docs/nx/nx9/ugdoc/html_files/nx_help/index.h...

 

I hope this help.

Jean Marcel
PLMPRO
www.plmpro.com.br

Re: NX and Hyper Threading

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
I would always recommend to turn it off. I had a customer recently that had just purchased new Dell systems and was getting load time differences compared to their old systems. As a test on the same new Dell, for a very detailed assembly, the load times were: With HyperThreading turned on: 10:43 With HyperThreading turned off: 06:14
Anthony Galante, Senior Support Engineer
PhoenxPLM
24 versions of NX installed: NX4 to NX12, plus TC11.2

Re: NX and Hyper Threading

Phenom
Phenom

Thanks for the input.

 

Basic test of build model and generate CAM operations don't show significant difference with it on or off (NX4)

 

I also ran the  blocks benchmark originally from  @Stefan_Pendl (I think) TestBlockPerformance.vb

 

Interesting my NX9 performance now matches the NX4 performance of my 8 year old Dual Xeon X5482 3.20GHz

 

Old machine 

NX v4.0.4.2
Test_1000_Blocks_v4.prt
Creating 1000 Blocks ...
Elapsed ... 25.323

 

New Machine

NX v9.0.3.4

Test_1000_Blocks_v9.prt

Creating 1000 Blocks ...
Elapsed ... 23.571

 

 

Re: NX and Hyper Threading

Phenom
Phenom

Further to this.

 

Has anyone used the Dell Precision Optimizer that ships with these workstations?

 

Any feedback would be appreciated.

 

Alex

Learn online





Solution Information