Cancel
Showing results for 
Search instead for 
Did you mean: 

NX drilling clearance plane/ offset ...

Pioneer
Pioneer

Hi, It might be very simple ... What I am trying to do is .. Drilling a part and I would like to actually start the drilling sequence with proper feed and speed let say 2 inches above the part top surface... because in some cases there will ba another part fixed with. so how can I offset the clearance plane or top surface to get the drilling to start ealier 

1 REPLY 1

Re: NX drilling clearance plane/ offset ...

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

The drilling (hole making) operations have a "top offset" cutting parameter, which can be used for this.

The clearance plane must be manually changed in the non-cutting-moves section to reflect this.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Learn online





Solution Information