Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

NX millturn project sample files for study.

Experimenter
Experimenter

Hi All.

 

I need NX9.0 millturn project sample files for study purpose. Where i can get the sample files?

 

Regards,

Mithun shet.

8 REPLIES 8

Re: NX millturn project sample files for study.

Legend
Legend

There are many things you can do with Mill-Turn machine. What specific operations or job type are you looking for ? Any specific industry parts ? or specific application ?

Re: NX millturn project sample files for study.

Experimenter
Experimenter

Hi,

 

Iam looking for aerospace engine casting type of parts. I have worked on 3 axis Milling and machined many parts. I do not have knowledge on NX turning and Millturn. I just want to study the case and understand the concept.

 

Thank you.

Re: NX millturn project sample files for study.

Legend
Legend

Get NX CAST installed. Some tutorials on Turning and Mill Turn are available.

Re: NX millturn project sample files for study.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

There is not CAST in NX9.

You would have to use the on-line "Learning Advantage" courseware:

https://training.plm.automation.siemens.com/mytraining/index.cfm

 

Also, look in the install tree for NX:

...\MACH\samples

...\MACH\tutorials  (I think this is the CAM Express stuff?)

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: NX millturn project sample files for study.

Be sure to go through the mill turn tutorial included in your system.

Menu > Help > Manufacturing Tutorials

Mark Rief
Retired Siemens

Re: NX millturn project sample files for study.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

And I (and Mark) didn't mention the tutorials available on the community site (I'm not sure if any directly apply to your situation, but...)

http://community.plm.automation.siemens.com/t5/NX-Manufacturing-Forum/ct-p/part-manufacturing

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: NX millturn project sample files for study.

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

 I would recommend you take a look at the sample provided in your install.

 

Navigate to where NX is installed.  As an example: ...NX9\MACH\samples\nc_simulation_samples

 

Look at the sim15_millturn files located there.  This should help you get started.

Re: NX millturn project sample files for study.


@td wrote:

 I would recommend you take a look at the sample provided in your install.

 

Navigate to where NX is installed.  As an example: ...NX9\MACH\samples\nc_simulation_samples

 

Look at the sim15_millturn files located there.  This should help you get started.


You can also get to these directly from with NX:

Menu > Help > Manufacturing Tutorials > Open a Sample Part

Scroll down to Simulation Examples.

Mark Rief
Retired Siemens

Learn online





Solution Information