Cancel
Showing results for 
Search instead for 
Did you mean: 

NX rate of calculation

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hello,
I would like to ask if it is possible to use the acceleration of the graphic card for calculations using OPENGL, CUDA?

Thank you

2 REPLIES 2

Re: NX rate of calculation

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
Nx for bitcoins maining?

Re: NX rate of calculation

I don't believe Siemens is using that for cam calculations but I may be wrong.  There is a lot of power in GPU processing and the prospect is very interesting.  I have built workstations in the past with three graphics in a SLI configuration and are close to making another with 3-4 1080 Ti cards.  Although those are not CAD cards they still perform decently for CAD/CAM and have a lot of processing power for grid computing such as Folding@home which I participate in.  What makes it interesting is multi-GPU's are absolutely way more powerful than any CPU for crunching grid work units.  Perhaps someone from development can chime in on this topic but I imagine if Siemens is working on alternative computing methods it is not being discussed publicly.    

NX 12.0.2

Learn online





Solution Information