Cancel
Showing results for 
Search instead for 
Did you mean: 

NX synchronization manager

Creator
Creator

Hello,

Currently I would like use NX synchronization manager to run main spindle and sub spindle of mill turn machine in same time. for example: when sub spindle is running, main spindle can load one new part then run. 

 

I am not sure I need pay for one more NX option to use synchronization manager to control 2 channel of mill turn machine?

 

Thanks!

2 REPLIES 2

Re: NX synchronization manager

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

If you have one of the following bundles then you are ok

NX10430, NX10440, NX10460, NX10470, NX12401, NX12411, NX12460, NX13411, NX13420, 

NX13421, NX13430, NX13440, NX14401, NX14410

 

If not you would need to purchase NX30434.

 

 

Frank Bartucci
NX CAM COE

Re: NX synchronization manager

I would try the samples and see if you get a license message or not.

 

Menu > Help > Manufacturing Tutorials > Open a sample part

>  sim15_millturn_setup_sinumerik_mm_dual_sync.prt

Select program SYNCH-GROUP

MB3 > Toolpath > Synchronize

 

Mark Rief
Retired Siemens

Learn online





Solution Information