cancel
Showing results for 
Search instead for 
Did you mean: 

NX10 Command Prompt

Pioneer
Pioneer

Hello,

How to find out "command prompt" from UGII FOLDER? BEFORE I can find it in the nx tool menu or UGII folder.

 

Thanks!

-----------------------------------------
UG3.0
UG6.0
NX10.0.35
NX11.0.1
UG_NX is my favorite !!!!!!
5 REPLIES

Re: NX10 Command Prompt

Pioneer
Pioneer

I find it out. Now it change file name " ug_convert_part.exe". But ,,,why when i want to open this. This window looks like "cmd" . dispearing fast!  Why?

 

Thanks!

 

-----------------------------------------
UG3.0
UG6.0
NX10.0.35
NX11.0.1
UG_NX is my favorite !!!!!!

Re: NX10 Command Prompt

To run a NX command window, go to Windows Start > All Programs > Siemens NX 11.0  > NX Tools > Command Prompt.

This should open a DOS style command window, with environment variables set for that version of NX.

start menu command prompt.jpg

Mark Rief
Retired Siemens

Re: NX10 Command Prompt

Valued Contributor
Valued Contributor

Hello,

 

This does not appear in windows 10 start menu.

Glenn Balon
Production: NX 11.0.1.11 MP6 Primarily CAM

Re: NX10 Command Prompt

Legend
Legend

Create the shortcut on desktop of Windows 10.

For this shortcut should be specified following properties:

Target   

cmd.exe /k "C:\Program Files\Siemens\NX 10.0\UGII\ugiicmd.bat" "C:\Program Files\Siemens\NX 10.0"

Start In

"C:\Program Files\Siemens\NX 10.0\UGII"

 

Re: NX10 Command Prompt

Valued Contributor
Valued Contributor

I found that running the batch file and then opening the command prompt also works. I will also make the shortcut. 

 

Thanks

Glenn Balon
Production: NX 11.0.1.11 MP6 Primarily CAM

Learn online





Solution Information