Cancel
Showing results for 
Search instead for 
Did you mean: 

NX10 and NX12

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi,

 

I have one problem. When I generate NC code in NX10 everythink is ok. But when I generate NC code in NX12 I get wrong output out (coordinats X,Y and Z are wrong). And PP is the same.

 

Can someone help me?

1 REPLY

Re: NX10 and NX12

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Note this is cross posted in NX Manufacturing forum - I'd suggest repsonding there

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Learn online





Solution Information