Cancel
Showing results for 
Search instead for 
Did you mean: 

NX11 Installation Applications

Creator
Creator

Hey,

 

I installed NX11 with the 11.0.2 update. After Installation I get a license from the server at school.

Now it seems i'm missing the applications pre post, Motion and Manufacturing. 

Since i used the same installation documents as my fellow students there shouldn't be a problem there.

Any help on what went wrong during the installation or if forgot something?

 

 

14 REPLIES

Re: NX11 Installation Applications

Legend
Legend

Try this
The employee must be on the right with the bundle

 

1.JPG

-----------------------------------------
NX 12.0.2.9 MP5 / Testing NX 1847
CanikSoft NC Post-Processing & G-Code Simulation
www.plast-met.com.tr
www.caniksoft.com

Re: NX11 Installation Applications

Creator
Creator

I have the bundles activated, used the Licensing tool, also activated in NX. image.png

Re: NX11 Installation Applications

Legend
Legend

Are you sure you are promoting the license and the correct license?

There is nothing else in mind

 

1.JPG

-----------------------------------------
NX 12.0.2.9 MP5 / Testing NX 1847
CanikSoft NC Post-Processing & G-Code Simulation
www.plast-met.com.tr
www.caniksoft.com

Re: NX11 Installation Applications

Creator
Creator

SahinSanli, i don't really get what you mean.

Re: NX11 Installation Applications

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

When you say you're missing applications, what does that actually mean?

The buttons for them are missing? Buttons are there, but the application doesn't start? You get an error?

 

Can you provide more detail or a screenshot?

The Academic bundles you've got has those functions, so you shouldn't be getting a license error.

 

 

 

Anthony Galante, Senior Support Engineer
PhoenxPLM
24 versions of NX installed: NX4 to NX12, plus TC11.2

Re: NX11 Installation Applications

Creator
Creator

The buttons are missing, i do not get an error. I tried different ways to open an application but all the buttons aren't there.
image.png

Re: NX11 Installation Applications

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
Ok you’re not missing any buttons but the tabs for the templates. Where NX is installed, there will be a folder called templates inside a folder called UGII. ...\UGII\templates Look in there for files with the extension .pax Compare what you have with the files a working system has.
Anthony Galante, Senior Support Engineer
PhoenxPLM
24 versions of NX installed: NX4 to NX12, plus TC11.2

Re: NX11 Installation Applications

Creator
Creator

The difference seems that the working files have ugs_... and the not working files nxdm_ugs_...  As far i can make something of it.
image.png

Re: NX11 Installation Applications

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

There should be an equal amount of files starting with ugs_ and with nxdm_ugs_.

ugs_ ... template only for native NX session without Teamcenter

nxdm_ugs_ ... template only for managed NX session with Teamcenter

Depending on your environment you should only need one or the other.

What does the NX log file tell you about the available applications?

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Learn online





Solution Information