Cancel
Showing results for 
Search instead for 
Did you mean: 

NX12 Part Boundaries

Pioneer
Pioneer

It seems NX 12 has completely reconfigured part boundary selection in planer milling operations. I truly miss NX 11 for that and several other reasons. Is there a way to activate the (old) NX 11 part boundary method and use it in NX 12?

3 REPLIES

Re: NX12 Part Boundaries

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @UGenius-not,

 

there is no way to return to the old boundary selection.

 

Would you mind sharing with us, what you are missing? Your feedback would help us.

 

Thanks in advance

Alexander

Lead Product Manager - Mold & Die

Re: NX12 Part Boundaries

Legend
Legend

It does take a minute or two to get used to...

But just like the interface switch going to NX9.0

 

Once you get used to it... You'll find it's better.

 

I had the same reaction

{Paul Schneider}, {CNC Programmer}, {DRT-Rochester}


Production: {NX11.0.2,MP5, NX12.0.2, MP4}

Re: NX12 Part Boundaries

Valued Contributor
Valued Contributor

There has been an IR/ER submitted.

 

The same thing happened when removing legacy hole operations,

Implemented where you could switch it back on to operate legacy hole operations.

 

IR #: 

8887867 

 IR 8887867 has been converted to ER 8887867; Desc: problems with the new planar mill boundary selection/definition in NX11

 

Re: NX 11.01.1.11 Planer Mill Functionality

EDS UG V3 -UG V15 UNIX; UGS UG V6 -UG V19 - NX-NX5 UNIX/MS; Siemens NX6-NX11 MS

Learn online





Solution Information