Cancel
Showing results for 
Search instead for 
Did you mean: 

NX12 annoying IPW display when selecting CAM operations

Creator
Creator

When reviewing and selecting toolpaths in manufacturing, NX will show me a pink solid facet body of the blank I am using for that operation. it completely blocks the view of my toolpath and I want it to go away. the only solution that "works" is right clicking, then "show 3d ipw", then "delete ipw". is there a setting I am missing somewhere that will disable the blank from view when selecting operations?

7 REPLIES 7

Re: NX12 annoying IPW display when selecting CAM operations

Siemens Phenom Siemens Phenom
Siemens Phenom

Try the following

Customer Defaults>>Manufactoring>>User Interface>>Operation Navigator tab>>Selection group>>uncheck 'Display Operation Geometry'

OK the dialog and restart NX. hope that this will resolve the issue.

Yours,

Eddy Finaro
NX CAM Product Manager
Siemens PLM

Re: NX12 annoying IPW display when selecting CAM operations

Creator
Creator
Thanks, I will try this as soon as i get in to work tomorrow and let you know.

Re: NX12 annoying IPW display when selecting CAM operations

Creator
Creator
thanks! it took a restart of nx for it to work.

Re: NX12 annoying IPW display when selecting CAM operations

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Would be nice that there was a different option to only hide the blank.

 

When I select an operation I would like to see the toolpath and the cutting area thats selected.

Especially with the new replay functions because when "Displey Selected Objects" is not active you have to select the operation, then display the toolpath and only then you can replay the toolpath.

 

Sven Voeten
Pre-sales NX CAM / Manufacturing Consultant
cards PLM Solutions

Re: NX12 annoying IPW display when selecting CAM operations

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Have you tried to change the display of the blank geometry through the customer defaults for manufacturing?

May be change "Customer Defaults => Manufacturing => Simulation & Visualization => IPW => IPW Translucency" to meet your needs.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: NX12 annoying IPW display when selecting CAM operations

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

That option is only working insid "Verify Tool Path".

 

I would like to be able to hide the blank when selecting the operation in the ONT and be able to replay the toolpath directly like you see in the picture below.

 

image.png

Sven Voeten
Pre-sales NX CAM / Manufacturing Consultant
cards PLM Solutions
Highlighted

Re: NX12 annoying IPW display when selecting CAM operations

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

So the solution would be to create an ER at GTAC, post its number and text here and we add me-to IRs for it.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Learn online





Solution Information