Cancel
Showing results for 
Search instead for 
Did you mean: 

NX1847 - Program order view issue - no operation

Gears Phenom Gears Phenom
Gears Phenom

Hello,

 

I found one problem but cant reproduce it. I didnt save prt, log file.

When creating operations they are visible in every view but not in program order view.

Did somebody met such problem?

I cant provide issue details to GTAC.

PR 9357330

 

thanks

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #
10 REPLIES 10

Betreff: NX1847 - Program order view issue - no operation

Valued Contributor
Valued Contributor
I had the same issue in NX12
Im not able to reproduce this behavior.
But i think if you create a tool in the toolnavigator-view and create then the operation also in the toolnavigator-view, the operation will not be displayed in every case in the programmnavigator-view.
Best regards

Production: {NX 10.0.3.5 MP18}
Testing: {NX 12.0.2.9 MP03}

Betreff: NX1847 - Program order view issue - no operation

Phenom
Phenom

I don't know the exact circumstances, but also copying an operation from another program and pasting into geometry group exhibits this behaviour. Not always, but often. IIRC clicking on the tree features in program order view does restore the missing items.

 

/Harri

 

Re: NX1847 - Program order view issue - no operation

Legend
Legend

I have had the same issue in NX12 to.I think it is about how many nx files are open.when I open a few different NX files than operations start to be invisible.this is happening program order view section. 

-----------------------------------------
NX 12.0.2.9 MP5 / Testing NX 1847
CanikSoft NC Post-Processing & G-Code Simulation
www.plast-met.com.tr
www.caniksoft.com

Re: NX1847 - Program order view issue - no operation

Creator
Creator

Is the NX1847 compared to the NX11 contour is a BUG??

 

11.png22.png

Re: NX1847 - Program order view issue - no operation

Valued Contributor
Valued Contributor
Could you share the part? Maybe there is a problem with the tolerance in the smoothing options...
Best regards

Production: {NX 10.0.3.5 MP18}
Testing: {NX 12.0.2.9 MP03}

Re: NX1847 - Program order view issue - no operation

Creator
Creator
Can you help me see what is the problem? Thank you

Re: NX1847 - Program order view issue - no operation

Valued Contributor
Valued Contributor
Hello
I don't get a better toolpath then yours. I tried but it won't get better.
You should report this to GTAC with your part in NX 11 so they can repeat the process.
Best regards

Production: {NX 10.0.3.5 MP18}
Testing: {NX 12.0.2.9 MP03}

Re: NX1847 - Program order view issue - no operation

Legend
Legend

Did you try clicking on the NC_PROGRAM, and then hit the right arrow. I have seen them get collapsed completely before.

 

 program.PNG

Glenn Balon
Production: NX 12.0.2 MP7 Primarily CAM

Re: NX1847 - Program order view issue - no operation

Creator
Creator
OK, thank you.

Learn online





Solution Information