Cancel
Showing results for 
Search instead for 
Did you mean: 

NX1847 Z-Level Tool Path Visual

Builder
Builder

Good day Experts,

 

I have created a tool path using z-level operation, and noticed that the " tool path replay" and "verify tool path"

have different presentation of tool path, when I tried to run the verify tool path, it seems ok,

the tool moves smoothly in circular pattern of what I am expecting. Is there any settings that I need to set to visualize the tool path correctly. 

 

Z-LEVEL_Replay_Tool_Path.jpgZ-LEVEL_Verify_Tool_Path.JPG

 

Thank you always

Jayson

3 REPLIES 3

Re: NX1847 Z-Level Tool Path Visual

Phenom
Phenom

Are you zooming in after using the "replay?" I have seen that happen when using replay further out and then zooming in. 

 

If "Display Selected Objects" is on in defaults, you can just select the path instead of using replay to see it. I leave off "Display Operation Geometry" to prevent the IPW from showing and blocking the path display. 

 

 

 

Display Selected Objects.PNG

Glenn Balon
Production: NX 12.0.2 MP10 Primarily CAM

Re: NX1847 Z-Level Tool Path Visual

Builder
Builder

Hi,

Thank you for the response,

I zoomed the object first then click the replay tool path, same as with the verify tool path.

I tried your suggestion by turning on the display selected object but the result is the same.

Z-LEVEL_Display_Selected_Object.JPG

Thank you always,

Jayson

Re: NX1847 Z-Level Tool Path Visual

Builder
Builder

Hi,

 

I tried to use analyze tool and the result is fine.

 

Z-LEVEL_Analyze_Tool.JPG

Learn online





Solution Information